DataPointConnection

Specifies whether data points on the chart are always connected with a line, will show a discontinuity in data by a break in the line, or are shown as unconnected markers. This property setting applies to all pens on the chart. If
Not Connected
is selected, pens without markers assigned on the
Pens
tab are not shown on the chart.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal