Search
FactoryTalk View ME Help
CloseValue
Type the value that will be written out when the button is pressed. The range is from -2,147,483,648 through 2,147,483,647.
This option is available when the
WriteOnClose
property is set to True.
All properties and connections
WriteOnClose
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal