Close Display connection
A write connection. Assign a digital tag to this connection to notify the data source that the pop-up alarm display has been closed.
When the application starts, this connection has a value of zero. If the pop-up alarm display specified in the
Alarm Setup
editor closes, the connection is set and held for the duration of the notification hold time, and is then reset to 0.Provide Feedback