ChartRadix

Specify the number base used to show numeric values on the chart. The available options are:
  • Decimal
  • Hexadecimal
  • Octal
This setting affects the numbers on the y-axis and the x-axis if XY plot is selected. If the number of decimal places on the
Y-Axis
tab is set to anything other than 0, it overrides the radix selection and shows numbers as decimals.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal