CaptionOnBorder

Specifies whether the object's caption or label can overlap the object's border.
This property has been created specifically to deal with objects in converted PanelBuilder 1400e applications, whose text may have overlapped the object's borders. This was possible because text labels on PanelBuilder 1400e objects were manually positioned. If the text label on an imported PanelBuilder 1400e object overlaps the object's border, the object's CaptionOnBorder property will be set to True on import. If the text on an imported object does not overlap the border, this property will be set to False.
For new objects, the default setting for this property is False.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal