ButtonAction
Select the type of action for the button:
- Normally opensends a value of 1 when the button is pressed, and a value of 0 when the button is released.
- Normally closedsends a value of 0 when the button is pressed, and a value of 1 when the button is released.
- Valuesends the value you assign to State 0 when the button is pressed and the value you assign to State 1 when the button is released.
If the button’s hold time is still in effect when the button is released, the second value is not sent until the hold time expires.
Provide Feedback