BufferSize
Specify the number of data points to be stored outside of the chart display area. The operator can view these data points by manual scrolling. The buffer size is limited to 32,767 data points. When the buffer is full, old data drops off.
Provide Feedback