Back style

Specifies the object background. The available options include:
  • Solid
    - Specifies the background color using the
    Back Color
    option.
  • Gradient
    - The object's background is filled with a linear gradient color.
  • Transparent
    - The object's background is not filled in and any objects behind it show through.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal