AuthorizedGroup
Select a group from the
AuthorizedGroup
list to grant the group access to the control object. If one group is selected from the list, all members of the selected group can be a supervisor of this object.The
AuthorizedGroup
list is generated from the groups that are added to FactoryTalk
Security.You do not need to add the Authorized Group to Runtime Security.
Provide Feedback