ActiveSymbol
Specifies the character to be shown in the
Active Symbol
column of the alarm list object, next to an alarm that is currently in alarm (active).The default symbol is an asterisk (*).
This property is only used if the DisplayActiveSymbol property is set to true.
Provide Feedback