ActiveAcknowledged

A read-only connection. Assign a tag or an expression to this connection. At runtime, when the tag or expression value is non-zero, the
Alarm List
shows alarms that are both active and acknowledged.
If you assign an expression to this connection, the application calculates the value of the expression and uses the result to determine whether to show active acknowledged alarms.
When this connection is assigned, it overrides the DisplayActiveAckedAlarms property.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal