AckSymbol
Specifies the character to be shown in the
Acknowledged Symbol
column of the alarm list object, next to an acknowledged alarm.The default symbol is an asterisk (*).
This property is only used if the DisplayAckSymbol property is set to true.
Provide Feedback