Ack connection

When the application starts, this connection has a value of zero.
When the operator acknowledges an alarm by pressing the
Ack Alarm
button, the application sends the alarm's trigger value (or bit position, for bit triggers) to this connection, and holds the value as long as the operator presses the button, or for the duration of the notification hold time, whichever is longer. Then the connection's value is reset to zero. Specify the hold time on the
Advanced
tab.
When the operator acknowledges all alarms by pressing the
Acknowledge All Alarms
button, the application sends the Acknowledge all value (specified in the
Use ack all value
box) to this connection, and holds the value as long as the operator presses the button, or for the duration of the notification hold time, whichever is longer. Then the connection's value is reset to zero.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal