Options on the Recipe tab of the RecipePlus Table Properties dialog box
The following table shows the options on the
Recipe
tab of the RecipePlus Table Properties
dialog box.Options | Descriptions |
|---|---|
Columns | Specify which columns to use, their width, and header text, if any. |
Select a column | Select a column to be edited:
|
Display column | Select this check box if you want the selected column to appear on the object. |
Width | Type the width in pixels of the selected column. The range is 0 - 1000. |
Header text | Type the text to show for the header of the selected column. |
Display | Choose whether or not to show headers and/or footers for the table at runtime. |
Display Header | Select this check box to show column headers on the object. |
Display Footer | Select this checkbox to show the footer on the table. |
List settings | Set how many lines each recipe ingredient will use, and how text will wrap in the table cells. |
Lines per item | From the drop-down list, select the number of lines each ingredient will use in the table. Range is from 1 to 10. |
Word wrap | Select this check box if you want the text to continue on the next line at the beginning of a new word. If this check box is cleared, the text continues on the next line whenever the maximum text length is reached, even if this occurs in the middle of a word or number. The maximum text length depends on the width of the object and the font size. |
User Input | Specify whether the table will be accessible to user input, or be view-only. |
View only | Select this checkbox if you want the table to be view-only. If the box is not checked, the operator will be able to make changes to the table. |
Provide Feedback