Set up recipe properties for the selector
Use the
Recipe
tab of the RecipePlus Selector Properties
dialog box to set up recipe properties for the object.To specify how recipes will be shown in the Recipe Selector
- In theGraphics Displayeditor, double-click the recipe selector to open itsPropertiesdialog box.
- Click theRecipestab.
- Specify whether headers will be shown.
- Specify the width of each of the selectors columns.
- Define the header text, if any.
Provide Feedback