Set up general properties for a RecipePlus selector

Use the
General
tab of the
RecipePlus Selector Properties
dialog box to set up how a RecipePlus selector looks.
To set up general options for a RecipePlus selector
  1. In the
    Graphics Display
    editor, double-click the object to open its
    Properties
    dialog box.
  2. Click the
    General
    tab.
  3. Specify the options.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal