Set up general properties for an ellipse or a circle object

Use the
General
tab of the
Ellipse Properties
dialog box to set up how an ellipse or a circle object looks.
To set up general properties for an ellipse or a circle object
  1. In the
    Graphics Display
    editor, double-click the ellipse or circle to open its
    Properties
    dialog box.
  2. On the
    General
    tab, specify the object appearance.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal