Set up general properties for a rectangle or square object

Use the
General
tab of the
Rectangle Properties
dialog box to set up how a rectangle or square object looks.
To set up general properties for a rectangle or square object
  1. In the
    Graphics Display
    editor, double-click the rectangle or square to open its
    Properties
    dialog box.
  2. On the
    General
    tab, specify the object appearance.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal