Set up general properties for a freehand object

Use the
General
tab of the
Freehand Properties
dialog box to set up how a freehand object looks.
To set up general properties for a freehand object
  1. In the
    Graphics Display
    editor, double-click the freehand object to open its
    Properties
    dialog box.
  2. On the
    General
    tab, specify the object appearance.
    TIP:
    Freehand objects have no edit mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal