Delete objects

You can delete one or more objects from a graphic display.
To delete objects
  1. Select one or more objects.
  2. Do one of the following:
    • From the
      Edit
      menu, select
      Delete
      .
    • Right-click the object and select
      Delete
      .
    • Press the
      Delete
      key on the keyboard.
      TIP:
      • To delete all the objects on a graphic display, from the
        Edit
        menu, select
        Clear All
        .
      • Delete does not use the clipboard. Use
        Undo
        to reverse an accidental deletion.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal