Set up states for a piloted control list selector

Use the
States
tab to set up how the piloted control list selector's appearance changes to match the value of the Indicator connection.
To set up states for a piloted control list selector
  1. In the
    Graphics Display
    editor, double-click the object to open its
    Properties
    dialog box.
  2. Click the
    States
    tab.
  3. From the
    Select state
    list, select
    State 0
    .
  4. Specify these properties for State 0:
    • Value
    • Caption, if any
    • Access. Whether the state can be selected by an operator, a remote controller, both, or neither
  5. Repeat steps 3 and 4 for each additional state.
Once you set up the properties for one state, you can copy and paste the state’s properties to another state or to all states.
TIP:
To add or remove a state without returning to the
General
tab, click
Insert State
or
Delete State
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal