Set up handshaking for a piloted control list selector

When the operator presses the
Enter
key, the application writes a value to the data source. Use Enter key handshaking to hold the value at the data source for a specific period of time to ensure it is read before the operator sends a new value to the Value connection.
To set up handshaking for a control list selector’s buttons
  1. In the
    Graphics Display
    editor, double-click the object to open its
    Properties
    dialog box.
  2. Click the
    Timing
    tab.
  3. Specify the handshaking settings to use with the
    Enter
    key.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal