Causes of runtime errors for an information message display

At runtime, the application logs errors about the information message display to diagnostics under this circumstance:
Unassigned connections
If the Ack connection is not assigned in the
Information Setup
editor and the
Acknowledge
button appears on the display, when the operator presses the
Acknowledge
button, the application logs an error.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal