Set up states for an Interlocked push button
Use the
States
tab of the Interlocked Push Button Properties
dialog box to set up states for the button.To set up states for an Interlocked push button
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theStatestab.
- From theSelect statelist, selectState 0.
- Specify these properties for State 0:
- General appearance
- Caption, if any
- Image, if any
- Repeat steps 3 and 4 for State 1.
Once you set up the properties for one state, you can copy and paste the state’s properties to another state or to all states.
Provide Feedback