Set up connections for an Interlocked push button
Use the
Connections
tab of the Interlocked Push Button Properties
dialog box to set up tags for the button.To set up tags for an Interlocked push button
- In theGraphics Displayeditor, double-click the button to open itsPropertiesdialog box.
- Click theConnectionstab.
- Assign a tag to this connection:ValueA read-write connection. Assign a tag to this connection. When the operator presses the button, the application writes the value for this button to the tag’s data source. The application also reads this tag to determine which state to display.Assign the same tag to the Value connection for eachInterlockedpush button in the group.
Provide Feedback