Create an interactive object

To use an interactive object, you need to create the object on a graphic display.
To create an interactive object
  1. In the
    Graphics Display
    editor, select the object from the
    Objects
    menu or toolbox.
  2. Drag the mouse to position and draw a rectangle the general size and location you want the object to be.
  3. Double-click the object to open its
    Properties
    dialog box.
  4. In the
    Properties
    dialog box, specify how the object looks, its behavior, and connections
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal