Audit trail list

Audit trail list shows the information about operator actions at runtime, including:
  • Occurred time
    - The local date and time when the software product records the action as having occurred.
  • Source
    - The name of the software product that logged the action in the audit log.
  • Location
    - The name of the computer, Windows CE device, or
    MobileView
    terminal on which the action took place.
  • Resource
    -
    Reserved
  • Username
    - The login ID of the user who is using the software product. This can be a
    FactoryTalk Security
    user or a
    Microsoft
    Windows
    user, depending on how the user logged into the software product that generated the audit record.
  • Message
    - Information about a specific operator action executed within the context of the running runtime application. For example, the message for a tag write will include the tag being modified, and the tag’s previous and new values.
Use the
Clear Audit Trail
button and the following
Key
buttons to interact with an audit trail list:
  • Move up
  • Move down
  • Page up
  • Page down
  • Home
  • End
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal