Set up general properties for an audit trail detail object

Use the
General
tab of the
Audit Trail Detail Properties
dialog box to specify how the audit trail detail object looks.
To set up general options for the audit trail detail object
  1. In the
    Graphics Display
    editor, double-click the object to open its
    Properties
    dialog box.
  2. On the
    General
    tab, specify the appearance, text, and the rest properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal