Set up general properties for an alarm status list

Use the
General
tab of the
Alarm Status List Properties
dialog box to set up general properties for an alarm status list.
To set up general properties for an alarm status list
  1. In the
    Graphics Display
    editor, double-click the alarm status list to open its
    Properties
    dialog box.
  2. On the
    General
    tab, specify the appearance, text, and the rest properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal