Set up connections for an alarm status list
Use the
Connections
tab of the Alarm Status List Properties
dialog box to set up connections for an alarm status list.To set up connections for an alarm status list
- In theGraphics Displayeditor, double-click the alarm status list to open itsPropertiesdialog box.
- On theConnectionstab, assign a numeric tag to the AlarmIdentifier connection.
TIP:
At runtime, the Alarm Identifier specified on the
Messages
tab of the Alarm Setup
editor will be written to the numeric tag assigned to the AlarmIdentifier connection only if the Use Alarm Identifier
check boxes are selected on the General
tab of the graphic object's Properties
dialog box and the Messages
tab of the Alarm Setup
editor. If the Alarm Identifier
column is blank on the Messages
tab of the Alarm Setup
editor and the Use Alarm Identifier
check boxes on both tabs are selected, zero will be written to the numeric tag.Provide Feedback