[STATUS] display
The
Graphics Libraries
folder contains displays called [STATUS].The [STATUS] display has an alarm status list object and the following buttons:
- Alarm Status Mode
- Silence Alarms
- Reset Alarm Status
- Home
- End
- Page Up
- Page Down
- Move Up
- Move Down
- Print Alarm Status
- Goto Display (to move to the[HISTORY] display)
- Close Display
You can use the [STATUS] display as it is or modify it to suit your needs. For example, you can change the appearance of the alarm status object and buttons in the display, or add or remove buttons.
You can also create your own graphic display containing an alarm status list object and buttons that you create, or copy and paste the objects on the [STATUS] display to the graphic display that you want the alarm status list graphic object to reside in.
Provide Feedback