Set up alarm conditions for an alarm list
Use the
Display
tab of the Alarm List Properties
dialog box to show the alarms in any or all of the following conditions:- Active and acknowledged
- Active and unacknowledged
- Inactive and acknowledged
- Inactive and unacknowledgedTIP:If you assign the connections on theConnectionstab of theAlarm List Propertiesdialog box, at runtime, those settings will override the settings on theDisplaytab.
To set up what alarms will be shown
- In theGraphics Displayeditor, double-click the alarm list to open itsPropertiesdialog box.
- On theDisplaytab, specify the alarm conditions to be shown in the alarm list at runtime.
- Specify whether the alarm will blink and what colors will be used to show the alarms.
Provide Feedback