[HISTORY] and [ALARM MULTI-LINE] displays
The
Graphics Libraries
folder contains displays called [HISTORY] and [ALARM MULTI-LINE].The [ALARM MULTI-LINE] display has an alarm list object and the following buttons:
- Acknowledge Alarm
- Acknowledge All Alarms
- Silence Alarms
- Move Up
- Move Down
- Close Display
The [HISTORY] display has a larger alarm list and the following buttons:
- Acknowledge Alarm
- Acknowledge All Alarms
- Silence Alarms
- Clear Alarm History
- Home
- End
- Page Up
- Page Down
- Move Up
- Move Down
- Print History
- Goto Display (to move to the [STATUS] display)
- Sort Alarms
- Close Display
You can use these displays as they are or modify them to suit your needs. For example, you can change the appearance of the alarm list object and buttons on the display, or add or remove buttons.
You can also create your own graphic display containing an alarm list object and buttons that you create, or copy and paste the objects on the [HISTORY] and [ALARM MULTI-LINE] displays to the graphic display that you want the alarm list graphic object to reside in.
Provide Feedback