Set up print options for a Print Alarm History button
At runtime, the operator presses a
Print Alarm History
button to print the contents of the alarm history.
TIP:
- You cannot print the alarm history and the alarm status at the same time.
- You can print alarms in landscape mode with a line printer, but only one alarm is printed per page.
- If you set up alarm messages in multiple languages, all messages, trigger labels and times are printed in the current application language.
To set up print options for a Print Alarm History button
- In theGraphics Displayeditor, double-click the button to open itsPropertiesdialog box.
- Click thePrinttab.
- Specify these properties for thePrintbutton:
- Column to print
- Column heading
- Column width
Provide Feedback