Set up general properties for an Alarm button

Use the
General
tab of the
Alarm Button Properties
dialog box to set up how an alarm button looks.
To set up general options for an alarm button
  1. In the
    Graphics Display
    editor, double-click the button to open its
    Properties
    dialog box.
  2. Click the
    General
    tab.
  3. Specify these properties:
    • General appearance
    • Touch margins
    • Audio (whether the button beeps at runtime)
Once you set up the options on the
General
tab, click the
Label
tab to set up a caption and image for the button.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal