[ALARM BANNER] display
The
Graphics Libraries
folder contains a display called [ALARM BANNER].The [ALARM BANNER] display has an alarm banner object and the following buttons:
- Acknowledge Alarm
- Silence Alarms
- Clear Alarm Banner
- Close Display
You can use the [ALARM BANNER] display as it is or modify it to suit your needs. For example, you can change the appearance of the alarm banner object and buttons on the display, or add or remove buttons.
You can also create your own graphic display containing an alarm banner object and buttons that you create, or copy and paste the objects on the [ALARM BANNER] display to the graphic display that you want the alarm banner graphic object to reside in.
Provide Feedback