Set up connections for a symbol indicator

Use the
Connections
tab of the
Symbol Indicator Properties
dialog box to set up a tag or expression for the object.
To set up tags and expressions for a symbol indicator
  1. In the
    Graphics Display
    editor, double-click the indicator to open its
    Properties
    dialog box.
  2. Click the
    Connections
    tab.
  3. Assign a tag or expression to this connection:
    Indicator
    A read connection. You can assign a tag or an expression to this connection.
    If you assign a tag, the application reads the value of the tag at the data source, assigns this value to the connection, and updates the object in the display to reflect the state corresponding to the value or least significant bit value (depending on the trigger type).
    If you assign an expression, the application calculates the value of the expression and updates the object’s display to reflect the state corresponding to the value or least significant bit value (depending on the trigger type).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal