Set up general properties for a symbol indicator
Use the
General
tab of the Symbol Properties
dialog box to set up how a symbol indicator looks.To set up general options for the symbol indicator
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theGeneraltab.
- Specify the options.
If the image is not a monochrome bitmap, or if the bitmap has been removed from the project, an X appears on the indicator.
Once you set up the options on the
General
tab, click the States
tab to specify how the object looks in each state at runtime.Provide Feedback