How the string display works at runtime

The string display shows the string value of the Value connection at the data source. The application clears the display before showing a new string.
Open graphic displays
When you open a display at runtime, the application reads the Value connection value and updates the display based on the value.
What is shown
  • If the Value connection is unassigned, the display is blank.
  • The application displays the number of characters (bytes) specified for the tag assigned to the Value connection. If a longer string is read from the connection, only the specified number of characters is shown.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal