Example: Use a scale
In this example, the scale object helps in visually determining the speed of a conveyor as depicted by a bar graph.
- Create a scale and change the number of minor ticks to 9.
- Set the back style to transparent.
- Place the scale on top of a bar graph.
As the bar graph fill changes, the value it represents can be determined by using the scale ticks as markers.
TIP:
If the scale disappears behind the bar graph, from the
Arrange
menu, select Bring to Front
.Provide Feedback