Set up connections for a Ramp button

Use the
Connections
tab of the
Ramp Button Properties
dialog box to set up tags for the button.
To set up tags for a Ramp button
  1. In the
    Graphics Display
    editor, double-click the button to open its
    Properties
    dialog box.
  2. Click the
    Connections
    tab.
  3. Assign a tag to these connections:
    Value
    A read-write connection. The application keeps a copy of the Value connection on the computer. When the operator presses the
    Ramp
    button, the application adds or subtracts the "Ramp value" amount (specified on the
    General
    tab) from the local Value connection value and writes the result to the Value connection tag’s data source.
    If the "Ramp value" amount is a floating point value and the Value connection is an integer tag, the application rounds the value before writing it to the connection.
    Ramp
    A read connection. Assign a tag or an expression. The application reads the connection to determine by what value the object will increase or decrease the data source.
    This connection is only used if the
    Use variable ramp
    check box on the
    General
    tab is selected.
    Limit
    A read connection. Assign a tag or an expression. The application reads the connection value to determine the highest or lowest ramp value the object can write to the data source.
    This connection is only used if the Use variable lower/upper limit check box on the
    General
    tab is checked.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal