Set up auto repeat for a Ramp button
If you set up auto repeat, when the operator presses and holds down the
Ramp
button, repeated button presses are registered until the operator releases the button. For each button press, the application sends the new ramped value to the data source.
TIP:
If the
Ramp
button is in auto repeat mode, the application ramps the value that was previously sent to the Value connection, rather than reading the connection from the data source and ramping the current connection value. This means that external changes to the Value connection are not recognized while the button is in auto repeat mode.To set up auto repeat for the Ramp button
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theTimingtab.
- Specify the auto repeat settings to use with theRampbutton.
Provide Feedback