Example: Use a Ramp button
This example shows you how to use two
Ramp
buttons together to create a raise/lower control.Create two
Ramp
buttons. Configure one button like this:- Caption: Raise
- Ramp type: Ramp up
- Ramp value: 1
- Upper Limit: 100
- Auto repeat rate: 5
Configure the second button like this:
- Caption: Lower
- Ramp type: Ramp down
- Ramp value: 1
- Lower Limit: 0
- Auto repeat rate: 5
Assign the same tag to each button’s Value connection. Create a numeric display object to view the tag assigned to the
Ramp
buttons’ Value connection.When the operator presses the
Raise
button, the tag assigned to the Value connection increases by one. If the operator holds down the button the value continues to increase at a rate of five times per second. If the operator presses the Lower
button the value decreases.Provide Feedback