Set up connections for a numeric display

Use the
Connections
tab of the
Numeric Display Properties
dialog box to set up tags and expressions for the object.
To set up tags and expressions for a numeric display
  1. In the
    Graphics Display
    editor, double-click the display to open its
    Properties
    dialog box.
  2. Click the
    Connections
    tab.
  3. Assign a tag or expression to these connections:
    Value
    You can assign a tag or an expression to this connection. The application reads the value of the Value connection’s tag at the data source and displays this value in the numeric display.
    If you assign an expression to this connection, the application calculates the value of the expression and shows the result in the numeric display.
    Polarity
    You can assign a tag or an expression to this connection. This connection determines whether or not a minus sign is shown. A minus sign is shown when this connection has a positive non-zero value. If this connection is assigned, it overrides the polarity of the Value connection’s value.
    If you assign an expression to this connection, the application calculates the value of the expression and uses the result to determine whether to display a minus sign.
    If the Polarity connection uses a tag with a floating point address, values less than .5 will be rounded down and values greater than or equal to .5 will be rounded up.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal