Set up general properties for a numeric display

Use the
General
tab of the
Numeric Display Properties
dialog box to set up how a numeric display looks.
To set up general options for a numeric display
  1. In the
    Graphics Display
    editor, double-click the object to open its
    Properties
    dialog box.
  2. Click the
    General
    tab.
  3. Specify the options.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal