Set up states for a Multistate push button
Use the
States
tab of the Multistate push button Properties
dialog box to set up states for the button.To set up states for a Multistate push button
- In theGraphics Displayeditor, double-click the button to open itsPropertiesdialog box.
- Click theStatestab.
- In theSelect statelist, clickState 0.
- Specify these properties for State 0:
- Value
- General appearance
- Caption, if any
- Image, if any
- Repeat steps 3 and 4 for State 1 and the Error state.
Once you set up the general, caption, and image properties for one state, copy and paste the state’s properties to another state or to all states.
Provide Feedback