Set up auto repeat for a Multistate push button
If you set up auto repeat, when the operator presses and holds down the push button, repeated button presses are registered until the operator releases the button. For each button press, the application sends the value for the next state to the data source.
To set up auto repeat for a Multistate push button
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theTimingtab.
- Specify the auto repeat settings to use with the push button.
Provide Feedback