How the Multistate push button works at runtime

When the operator first presses the button, it changes from State 0 to State 1 and sends the State 1 value to the data source. When the operator presses the button a second time, it changes from State 1 to State 2 and sends the State 2 value to the data source. Thus the state is incremented by one for each button press. When the button is in the last configured state and the operator presses it, it changes to State 0 and sends the State 0 value to the data source.
The
Multistate
push button’s behavior at runtime also depends on how you set up the
Next state based on
option, auto repeat options, and controls.
Change states
The application uses the
Next state based on
option (specified on the
General
tab of the
Multistate Push Button
dialog box) to determine how to change the button’s state.
  • When the operator presses the button, if
    Next state based on
    is set to Value, and the control’s value does not match any of the states’ values, the button is set to State 0 and the application writes the State 0 value to the data source.
Use auto repeat
Set up the Auto repeat rate and Auto repeat delay options on the
Timing
tab of the
Multistate Push Button
dialog box.
  • When the operator presses the button, the auto repeat delay starts timing. The application continues timing until the operator releases the button or until the time reaches the Auto repeat delay time. If the Auto repeat delay time is reached, the button goes into auto repeat mode until the operator releases the button. Once in auto repeat mode, the application uses the Auto repeat rate option to determine the number of button presses per second to send to the data source.
  • When in auto repeat mode, the application does not read the Value connection to determine the next value to write out, regardless of the
    Next state based on
    setting. The application uses the last value written out to determine the next value to write out.
Use controls
  • If you assign just the Value connection and not the Indicator connection, the button’s pressed state is shown as soon as the button is pressed. The feedback for this connection is local and immediate. It does not necessarily reflect the Value connection’s value in the data source.
  • If you assign the same tag to the Value and Indicator controls, at runtime the shown button state is based on the Indicator connection. If network traffic is heavy, the display response might be delayed.
  • If the Indicator connection value is a floating point value, the application rounds the value to the nearest integer to determine the state to display.
Start projects
When you open the display at runtime, the application reads the Value connection and sets the button to this state, regardless of the
Next state based on
setting.
Open and close graphic displays
  • When you open a display at runtime, the application reads the Value connection value, but does not write the value to the data source.
  • When you open a display at runtime, the application reads the Indicator connection value and updates the display based on the value, unless the Value connection is unassigned.
  • When you close a display at runtime, if the button is in auto repeat mode, the button is released and the application writes the current value to the Value connection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal