Set up general properties for a multistate indicator

Use the
General
tab of the
Multistate Indicator Properties
dialog box to set up how a multistate indicator looks.
To set up general options for a multistate indicator
  1. In the
    Graphics Display
    editor, double-click the object to open its
    Properties
    dialog box.
  2. Click the
    General
    tab.
  3. Specify the options.
Once you set up the options on the
General
tab, click the
States
tab to specify how the object looks in each state at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal