Set up states for a Momentary push button

Use the
States
tab of the
Momentary Push Button Properties
dialog box to set up states for the button.
To set up states for a Momentary push button
  1. In the
    Graphics Display
    editor, double-click the object to open its
    Properties
    dialog box.
  2. Click the
    States
    tab.
  3. From the
    Select state
    list, select
    State 0
    .
  4. Specify these properties for State 0:
    • Value (for Momentary push buttons with the Value button action); when the Indicator connection changes to this value, the button's appearance changes to the settings you specify for the state.
    • General appearance
    • Caption, if any
    • Image, if any
  5. Repeat steps 3 and 4 for State 1 and the Error state.
Once you set up the properties for one state, you can copy and paste the state’s properties to another state or to all states.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal